Mouser Electronics and Navitas Semiconductor Announce Global Distribution Agreement
April 24, 2023 – Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, announces a global distribution agreement with Navitas Semiconductor, the only pure-play, next-generation power semiconductor company and industry leader in gallium nitride (GaN) power ICs and silicon carbide (SiC) technology. According to the agreement, Mouser will offer customers Navitas' range of GaNFast™ and GaNSense™ power ICs, in addition to the GeneSiC™ range of SiC power MOSFETs and diodes. These highly-efficient semiconductors enable high-frequency performance for applications including electric vehicles, fast charging devices, consumer electronics, alternative energy and industrial solutions.
"Mouser is pleased to add this strong industry leader to our line card, and to deliver these innovative power devices to our customers," said Kristin Schuetter, Mouser's Vice President of Supplier Management. "Design engineers now have easy access to Navitas' advanced components, backed by Mouser's unsurpassed customer service and best-in-class logistics. We're looking forward to a very successful partnership."
"Adding GaNFast parts to the existing GeneSiC portfolio greatly amplifies the awareness, interest and ultimately revenue for Navitas via Mouser's established and successful distribution platform," said David Carroll, Senior Vice President Worldwide Sales at Navitas Semiconductor. "Next-gen products, ease-of-use, immediate availability and great tech support mean that power designers can quickly deliver high-quality prototypes with both SiC and GaN, on time and ready for mass production."
The GaNFast Power ICs enable switching frequencies six-times higher than discrete GaN solutions, enabling an increase in system energy savings, while reducing system size and weight. GaNFast power ICs are easy to use and compatible with a range of popular topologies and controllers. GaNFast power ICs monolithically integrate GaN power, drive, and control, to create an easy-to-use, high-speed, high-performance 'digital-in, power-out' building block. GaNFast power ICs enable up to 3x faster charging in half the size and weight of old, silicon-based power electronics, or 3x more power without a size or weight increase.
GaNFast Power ICs with GaNSense technology integrate critical, real-time, autonomous sensing and protection circuits which further improve Navitas' industry-leading reliability and robustness. These revolutionary single-package solutions reduce component count and footprint compared to existing discretes, which cuts system cost, size, weight, and complexity. Featuring a supply voltage range of 5.5 V to 24 V, GaNFast power ICs are ideal for a variety of consumer and enterprise applications.
The GaNFast family of power ICs offers multiple efficiency and reliability benefits in easy-to-use, low-profile, low-inductance, industry-standard PQFN packages. These devices enable fast time-to-prototype and fast time-to-revenue and are designed to enable the next generation of soft-switching topologies while maximizing GaN's high-speed, MHz+ fast-switching capability. These high-efficiency devices are suitable for mobile and data center applications, as well as industrial motor drives.
To learn more about power ICs from Navitas Semiconductor, visit https://www.mouser.com/manufacturer/navitas/.
Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.
2023 - Mouser Electronics, qui appartient à la famille d’entreprises Warren Buffett Berkshire Hathaway, est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits et technologies de ses partenaires pour les ingénieurs concepteurs et les acheteurs. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 27 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.
2023 - Navitas Semiconductor is the only pure-play, next-generation power-semiconductor company, founded in 2014. GaNFast™ power ICs integrate gallium nitride (GaN) power and drive, with control, sensing, and protection to enable faster charging, higher power density, and greater energy savings. Complementary GeneSiC™ power devices are optimized high-power, high-voltage, and high-reliability silicon carbide (SiC) solutions. Focus markets include mobile, consumer, data center, EV, solar, wind, smart grid, and industrial. Over 185 Navitas patents are issued or pending. Over 50 million GaN units have been shipped with zero reported GaN field failures, and Navitas introduced the industry’s first and only 20-year warranty. Navitas is the world’s first semiconductor company to be CarbonNeutral®-certified.
Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.