Nexperia’s NEH2000BYJ PMIC, Now Available at Mouser, Offers High-Performance Energy Harvesting for Low-Power Applications
April 25, 2023 – Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is now stocking the NEH2000BYJ energy harvesting power management integrated circuit (PMIC) from Nexperia. The NEH2000BYJ PMIC harvests energy generated by a photovoltaic (PV) cell, which in turn charges a rechargeable battery. The new PMIC from Nexperia is an ideal choice for low-power applications, including wireless Internet of Things (IoT) devices, wearable devices, smart remote controls, and industrial and environmental monitoring.
The Nexperia NEH2000BYJ energy harvesting PMIC, now available at Mouser, includes pre-sets on the chip, making the implementation of energy harvesting designs simpler. This offers an unprecedented ease-of-use for engineers. Even with limited energy harvesting knowledge, it is possible to quickly integrate and deploy high-performing energy harvesting in new product designs.
Nexperia’s advanced maximum power point tracking (MPPT) uses an embedded hill-climbing algorithm to deliver the maximum power to the load. The MPPT is designed to be independent of specific characteristics of the harvesters, therefore any harvester that fits the specifications of the chip can be used. In addition, the MPPT circuit can detect the maximum power point with an interval of 0.7 seconds resulting in maximum efficiency in various environments where energy can rapidly change over time. The MPPT functions autonomously and requires no pre-programming. Consequently, self-optimization makes it no longer required to have an extremely detailed understanding of the fluctuating environment.
The NEH2000BYJ PMIC offers a harvesting power range from 35 μW to 2 mW and is available in a compact, 16-lead 3.0 mm × 3.0 mm QFN package, ideal for space-constrained applications.
To learn more about the NEH2000BYJ energy harvesting PMIC from Nexperia, visit https://www.mouser.com/new/nexperia/nexperia-neh2000byj-pmic/.
Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.
2023 - Mouser Electronics, qui appartient à la famille d’entreprises Warren Buffett Berkshire Hathaway, est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits et technologies de ses partenaires pour les ingénieurs concepteurs et les acheteurs. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 27 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.
2023 - Nexperia est un leader mondial dédié dans les composants discrets, logiques et MOSFET. Auparavant partie intégrante des produits NXP Standard, Nexperia se concentre sur l'efficacité, produisant des composants semi-conducteurs fiables en permanence en grande série. Le vaste portefeuille de la société répond aux normes strictes fixées par l'industrie automobile. Les petits boîtiers à la pointe de l'industrie, produits dans les usines de fabrication de Nexperia, combinent l'efficacité énergétique et thermique aux meilleurs niveaux de qualité de leur catégorie.
Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.