Engineering eVTOL Urban Air Mobility: Less Noise, More Power and Safety
Image Source:
Anastasiia/Stock.adobe.com; generated with AI
By Mouser Technical Content Staff
Published March 27, 2026
Over the next three to five years, urban air mobility (UAM) companies aim to provide transportation services between airports and central business districts in a handful of policy-forward regions (Figure 1).[1] However, their ability to scale will hinge on quiet operations, megawatt-class vertiports (i.e., specialized infrastructure for vertical takeoff and landing), and airspace rules that earn public trust.
This article examines how expanding vertiport infrastructure, evolving global certification paths, and early demonstration routes will lay the groundwork for scalable, dependable UAM services worldwide.
Figure 1: Early corridors will connect airports and central business district vertipads on predictable schedules. (Source: ViskBx/stock.adobe.com; generated with AI)
From Demos to Day-One Routes
The last decade has seen dozens of demonstration flights from startups and established aviation companies. But in the past two years, these flights have progressed from impressive displays to test flights intended to prove the viability of electric vertical takeoff and landing (eVTOL) in everyday environments.
For example, Joby and All Nippon Airways staged multiple demonstration flights at Expo 2025 Osaka from a purpose-built vertiport, offering a first look at seamless pad-to-pad operations rather than isolated test hops.[2] Such demonstrations are not important simply because an eVTOL had a successful flight. Instead, they show a level of readiness among infrastructure, procedures, and operational rules that is ushering in a new type of transportation. In the Persian Gulf, Abu Dhabi Airports and Skyports Infrastructure broke ground on a network of vertiports at Zayed International Airport and Al Bateen Executive Airport, striving to build a multi-site grid.[3]
Quiet by Design
While helicopters are a valuable mode of transportation worldwide, they are not suited to the UAM vision. Their rotor blades displace air at high speed, producing intrusive noise up to 100dBA.[4]
In NASA-supported tests, Joby’s aircraft measured approximately 45dBA at 500m (1,640ft) in overflight, and under 65dBA at roughly 100m (328ft) in liftoff and landing.[5] For context, 45dBA is close to a suburban nighttime soundscape, and 65dBA is the approximate loudness of a typical office environment.[6]
The Vertiport as a Micro Power Plant
In a 2023 study, the US Federal Aviation Administration (FAA), in collaboration with the National Laboratory of the Rockies (NLR; formerly the National Renewable Energy Laboratory), found that even modest vertiports will require a megawatt or more of high-quality power with fast‑charge profiles, even before scaling to multiple vertipads (Figure 2).[7] These vertiport power stations will be like a cluster of automotive DC fast chargers running simultaneously, only with aviation-grade interlocks, redundancy, and thermal management.
Figure 2: Even smaller vertiports will require significant charging infrastructure. (Source: Anna/stock.adobe.com; generated with AI)
Underpinning these power requirements are two frameworks that are converging quickly: SAE J3271 Megawatt Charging System (MCS) defines a megawatt-class DC interface and communications layer that spans heavy vehicles and electric aviation use cases, enabling interoperability and safety messaging across vendors.[8] NFPA 855 and UL 9540A provide standards regarding siting, spacing, ventilation, and fire suppression of energy storage systems.
Certification
Though some eVTOLs take forms similar to those of helicopters or airplanes, regulatory bodies are not forcing them into those classifications. In the US, the FAA has certified them as powered-lift aircraft, a historic first for a new civil category since helicopters.[9] This guidance clarifies the type, production, and airworthiness paths manufacturers must document to prove compliance.
Further, the FAA’s Modernization of Special Airworthiness Certification (MOSAIC) final rule expands the definition of light-sport aircraft to include rotor-based and powered-lift aircraft. However, commercial operators must still certify their crafts under airworthiness and air carrier rules.[10]
The European Union Aviation Safety Agency’s (EASA’s) Special Condition for VTOL (SC‑VTOL) and its evolving Means of Compliance offer a parallel airworthiness path, including guidance around thermal runaway risk management for high-energy batteries. This alignment between the US and EU could lower costs for global fleets.[11]
Airspace Integration
Initial UAM corridors will act as bus lanes in the sky, establishing routes and performance‑based traffic volumes with air traffic controllers monitoring flight plans and airspace. The FAA’s UAM Concept of Operations v2.0 outlines how services scale through digital intent sharing, performance-based separation, and network operations that include redundant links, health monitoring, and real‑time constraints.[12]
On the ground, operators will run network operations control centers (NOCCs) that supervise fleet health, charge cycles, weather, and pad status.[13] These will be similar to airport operations rooms or power-utility control centers, featuring boards, exception alerts, and disciplined procedures that enable a small team to manage a large, distributed fleet.
Safety, Fire Science, and the “Worst Day” Design
Public acceptance of widespread UAM adoption will not hinge on the best day of flights but on the worst. As a result, NFPA 855 and UL 9540A are prominent in vertiport design. UL 9540A’s large-scale fire-propagation test data give fire marshals evidence to set separation distances, ventilation requirements, and suppression tactics for stationary storage systems used to buffer the grid and enable fast turnarounds.[14]
Engineers will need to integrate robust environmental protections into battery rooms, including gas detection, deflagration panels where allowed, ducting that avoids recirculation to public areas, and fail‑safe charging behaviors. These processes will require forensic traceability from the start, including time-stamped charge profiles, connector states, and battery management systems (BMS) events, so root causes survive the heat of catastrophes and meaningfully improve the next design.
The Ramp to Scale
As UAM systems roll out in early-adopter cities, expect piloted, scheduled services on just a few corridors, with pricing that seems closer to a premium ride-share than private aviation. In Dubai and Abu Dhabi, the first routes will double as living labs to pressure-test operations, passenger processing, and multimodal handoffs. In the US, attendees of the 2028 Summer Olympics may have the opportunity to take an air taxi to the games. Archer Aviation plans to deploy its Midnight eVTOL fleet to Los Angeles to ferry passengers and emergency responders.[15]
Conclusion
Urban air mobility will succeed when it’s no longer novel. UAM systems will be ready to scale when eVTOL aircraft takeoffs and landings are no more extraordinary than those of passenger jets. The next three to five years will be less about wild new prototypes and more about integrating standards, infrastructure, and trust.
This blog was generated with assistance from Copilot for Microsoft 365 and adapted from Engineer the Sky – The Tech Between Us.
Sources
[1] https://www.eveairmobility.com/alt-air-teams-up-with-eve-air-mobility-and-skyports-infrastructure-to-advance-electric-aviation-in-new-south-wales-and-queensland/; https://www.helihub.com/2026/03/09/skydrive-completes-first-demo-flights-in-tokyo/
[2] https://www.aerotime.aero/articles/joby-evtol-aircraft-flight-expo-2025-japan; https://www.jobyaviation.com/news/joby-ana-holdings-kickoff-next-phase-of-air-taxi-development-in-japan-with-public-flight-demonstration-at-the-expo-2025-osaka-kansai-japan
[3] https://www.ainonline.com/aviation-news/futureflight/2025-11-12/abu-dhabi-airports-and-skyports-confirm-vertiport-plans
[4] https://www.sandiegocounty.gov/content/dam/sdc/pds/ceqa/Soitec-Documents/Final-EIR-Files/references/rtcref/ch2.6/2014-12-19_NPS2007.pdf
[5] https://newatlas.com/aircraft/nasa-joby-evtol-noise/
[6] https://ehs.yale.edu/sites/default/files/files/decibel-level-chart.pdf
[7] https://docs.nrel.gov/docs/fy24osti/86245.pdf
[8] https://www.anl.gov/sites/www/files/2023-03/MCS_FAQs_Final_3-13-23.pdf
[9] https://www.faa.gov/media/80526
[10] https://www.faa.gov/newsroom/MOSAIC_Final_Rule_Issuance.pdf
[11] https://www.easa.europa.eu/en/document-library/product-certification-consultations/special-condition-vtol
[12] https://www.faa.gov/sites/faa.gov/files/Urban%20Air%20Mobility%20%28UAM%29%20Concept%20of%20Operations%202.0_1.pdf
[13] https://www.supernal.aero/media/documents/Chakrabarty_Hosagrahara_Lei-Design_of_UAM_Network_and_Ecosystem.pdf
[14] https://www.ul.com/services/ul-9540a-test-method
[15] https://la28.org/en/newsroom/archer-selected-as-official-air-taxi-provider-of-la28-games.html
Author Bio
Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.