Mouser Announces Global Distribution Agreement with AIRMAR to Deliver Rugged Industrial and Environmental Sensor Solutions

Pour publication immédiate

Retrouvez-nous sur


August 20, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a new global distribution agreement with Amphenol Company, AIRMAR Technology, a world leader in the design and manufacture of high-performance sensors for marine and industrial applications. AIRMAR specializes in advanced ultrasonic transducers, electromagnetic flow sensors, and sensor monitoring systems targeted at commercial fishing, meteorology, ocean survey, and industrial process control markets.

Mouser will be stocking a wide range of AIRMAR solutions, including their WeatherStation® portfolio. The ultrasonic WeatherStation instruments provide accurate, reliable weather data from a rugged, compact design with no moving parts. These all-in-one multisensors can measure real-time apparent wind speed and direction, air temperature and calculated wind chill, barometric pressure, relative humidity, calculated dew point and heat index. The WeatherStation instruments elevate environmental sensing to the next level with the measurement of movement factors such as position, speed over ground (SOG) and course over ground (COG), rate-of-turn, and pitch and roll. AIRMAR Ultrasonic WeatherStation Instruments feature an integrated internal compass and GPS, enabling the unique measurement of dynamic true wind speed and direction from marine- and land-based mobile platforms. A 3D compass with dynamic stabilization provided by the three-axis rate gyro enhances heading accuracy in heavy pitch and roll conditions.

AIRMAR's AIRDUCER® ultrasonic industrial transducers, also available from Mouser, are suitable for a wide variety of applications and environments. These transducers deliver proven non-contact sensing performance for level and flow measurement of liquids or bulk solids, for process control in distance measurements, part monitoring, and proximity sensing. The AIRDUCER ultrasonic industrial transducers are rated IP68 and have no moving parts to wear out, so no maintenance is needed. Unlike most alternative measurement solutions, these ultrasonic transducers can detect clear, transparent or shiny objects and are unaffected by color. They operate within a frequency range of 15 kHz to 1 MHz and achieve a sensing range from 5 cm (2 in) to 60 m (196.85 ft).

To learn more about AIRMAR, visit https://www.mouser.com/manufacturer/airmar/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

À propos de Amphenol AIRMAR

2026 - Amphenol AIRMAR est un leader mondial de la conception et de la fabrication de capteurs haute performance pour les applications industrielles et marines. Il fabrique des transducteurs à ultrasons avancés, des capteurs de flux électromagnétique, des instruments WeatherGear® et des systèmes de surveillance de capteurs dans diverses applications. Les marchés appropriés pour ces produits comprennent la pêche maritime récréative, la pêche commerciale, la météorologie, les études océaniques, le contrôle des procédés et la détection de proximité.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764