Mouser Electronics and Atmosic Technologies Announce Distribution Agreement

Pour publication immédiate

Retrouvez-nous sur


June 28, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, announces a distribution agreement with Atmosic Technologies, a leading manufacturer of ultra-low-power wireless solutions for Internet of Things (IoT) applications. According to the agreement, Mouser will offer customers Atmosic's range of high-performance Bluetooth® 5 Systems-on-Chip (SoCs). Atmosic's exceptional low-power SoCs support a range of applications, including industrial asset-tracking solutions, sensors, medical devices, personal wearables, and automotive accessories.

The ATM32x1 SoCs from Atmosic combine a Bluetooth 5-compliant radio with an Arm® Cortex® M0 application processor. These devices support operation from a variety of energy harvesting sources, including RF, photovoltaic, thermoelectric generator (TEG), and motion. The ATM32x1 devices also support innovative wake-up mechanisms to enable further reduction in power consumption. The ATM22x1 Bluetooth 5 SoCs offers many of the same advanced power management features, but does not include energy harvesting. These high-performance, low-power SoCs are designed to extend the battery life of IoT devices, as low-duty cycle operation support allows IoT systems to run longer without battery replacement. Both the ATM32x1 and ATM 22x1 feature 256 K ROM, making them ideal for super high-volume applications, They also have a an external Flash interface for applications that require additional external Flash support.

The ATM3202 Bluetooth 5 SoC is an extremely low-power solution in a 40-pin 5mm2 QFN package. Featuring sophisticated power management and energy harvesting, the ATM3202 SoC provides exceptional performance for home automation, remote control and asset tracking applications. The ATM2202 Bluetooth 5 SoC boasts a fully integrated RF front-end and I2C, SPI, UART, PWM, and GPIO interfaces. The SoC also features a sensor hub, a true random number generator (TRNG) and a digital microphone input (PDM). Both the ATM3202 and ATM 2202 feature embedded Flash, ideal for applications looking for the flexibility available through Flash but have size constraints that don’t allow for external Flash.

To learn more about low-power SoCs from Atmosic, visit https://www.mouser.com/manufacturer/atmosic/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

About Atmosic Technologies

2026 - Atmosic™ Technologies is an innovative fabless semiconductor company, designing ultra-low power wireless and energy harvesting solutions to dramatically reduce and disrupt device dependency on batteries, aiming to deliver forever battery life and the battery-free connected Internet of Things. The company’s products enable the IoT device ecosystem—designers and manufacturers, as well as end users and those responsible for deployments—to dramatically lower costs and efforts associated with maintaining the growing Internet of Things in Personal, Home, Auto, Healthcare, Industrial, Enterprise and Smart Cities segments. In addition to these tangible business advantages, Atmosic aims to reduce ecological impacts with its vision of dramatically reducing battery consumption in the Internet of Things.


Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764