Ezurio's Vela IF310 Multiprotocol Modules, Now at Mouser, Feature Next Gen Audio-Centric Bluetooth Core 6.0 Classic and LE Connectivity

Annonce de nouveaux produits

Retrouvez-nous sur


Learn more about the Vela IF310 modules
Learn more about the Vela IF310 modules

May 20, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the Vela™ IF310 multiprotocol modules from Ezurio. The Vela IF310 modules are based on the Infineon Technologies AIROC™ CYW55310 system on chip (SoC) and combine Bluetooth® Classic (BR/EDR) and the complete Bluetooth 6.0 Low Energy (LE) feature set. Engineered for high-reliability environments, the Vela IF310 modules deliver a low-risk, fast-to-market platform for applications including fitness equipment, automotive infotainment, POS and barcode scanners, and medical monitors.

The Ezurio Vela IF310 modules, now at Mouser, include LE audio with LC3, isochronous channels, Auracast, LE-coded, and two MPHY and advertising extensions, allowing legacy classic designs to be updated with a single module. The Vela IF310 modules feature a powerful MCU subsystem with a 192 MHz Arm® Cortex-M33 processor, 2 MB ROM, and 768KB SRAM, with TrustZone® and CryptoCell™-312 security. The Vela IF310 series also offers a rich set of audio interfaces, including dual TDM/I2S plus PCM for HFP, A2DP, LE Audio, and multi-stream use cases. With flexible software hosting, the modules can be seamlessly integrated into automotive, retail, and medical applications. The Vela IF310 modules offer a single 12 × 16 mm2 footprint with multiple antenna variants, including integrated Ignion antenna, MHF4 connector, or RF trace pad, along with DVKs to make it easy to evaluate in real-world environments. The Vela IF310 modules minimize downtime in clinical settings and ensure interference-resistant audio in industrial spaces, with a rugged operating temperature range of -40°C to +85°C.

Ezurio Vela IF310 development kits provide a platform for rapid development and testing of the Vela IF310 modules. Two variations are available: part # 453-00390-K1 features an integrated chip antenna, and part # 453-00391-K1 includes an MHF4 connector for an external antenna. Featuring on-board headers and jumpers, the development kits provide a convenient way to isolate power and signal nets for debugging and power measurements.

To learn more, visit https://www.mouser.com/new/ezurio/ezurio-vela-if310-modules/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

About Ezurio

2026 - Ezurio turns design possibility into reality with a comprehensive range of RF modules, system-on-modules, single-board computers, internal antennas, IoT devices, and custom solutions. With decades of engineering expertise, Ezurio provides solutions that reduce development costs and time to market. Ezurio's global reach and unmatched support are backed by a resilient global supply chain that gives our customers the stability to overcome every design challenge with confidence. Turn design possibility into reality with Ezurio, your connectivity expert.

Laird Connectivity and Boundary Devices are now Ezurio.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764