Now at Mouser: Monolithic Power Systems (MPS) MPQ4242B-AEC1 Fully Integrated Power Delivery IC for Automotive Applications

Annonce de nouveaux produits

Retrouvez-nous sur


Learn more about the MPQ4242B-AEC1 PD IC
Learn more about the MPQ4242B-AEC1 PD IC

May 12, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the MPQ4242B-AEC1 fully integrated power delivery (PD) IC from Monolithic Power Systems (MPS). The MPQ4242B-AEC1 features an integrated buck-boost converter with four power switches and a USB PD controller. The MPQ4242B-AEC1 is AEC-Q100 Grade 1 qualified and designed for USB Type-C® sourcing ports in automotive applications.

The Monolithic Power Systems (MPS) MPQ4242B-AEC1 PD IC, now available at Mouser, supports up to 5-amps of continuous output current (IOUT) over the specified input supply range. The MPQ4242B-AEC1 features a USB Type-C port that supports USB PD revision 3.1 with a programmable power supply (PPS). The MPQ4242B-AEC1 is backward-compatible with dedicated charging port (DCP) schemes for battery charging specification (BC1.2), 3A divider mode, and 1.2V/1.2V mode. In addition, the MPQ4242B-AEC1 supports QC 2.0/3.0 and the Huawei Fast Charge Protocol (FCP) mode. When battery voltage (VBATT) is low or in the event of over-temperature (OT), the MPQ4242B-AEC1 provides a configurable PD power management state machine.

The MPQ4242B-AEC1 also includes fault condition protections, including input/output (I/O) pin short protection for the BUS and VIN pins, CC overcurrent protection (OCP), current limiting with hiccup mode, output overvoltage protection (OVP), and thermal shutdown. The MPQ4242B-AEC1 is delivered in a QFN-22 (4 x 5 mm2) package and requires readily available, standard external components.

The MPS EVQ4242B-VE-00A evaluation board, also available from Mouser, provides a demonstration and development platform for the MPQ4242B-AEC1. The evaluation board features a pre-mounted MPQ4242B-AEC1, along with the required components and headers enabling access to key signals. The EVQ4242B-VE-00A evaluation board provides an example application circuit, allowing rapid prototyping when incorporated into existing designs.

To learn more, visit https://www.mouser.com/new/monolithicpowersystems/mps-mpq4242b-aec1-power-delivery-ic/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

About Monolithic Power Systems (MPS)

2026 - Monolithic Power Systems (MPS) provides small, highly energy-efficient, easy-to-use power solutions for systems found in industrial applications, telecom infrastructures, cloud computing, automotive, and consumer applications. MPS creates cutting-edge solutions to improve the quality of life with green, easy-to-use products.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764