Mouser Now Stocking New Omron Electronics E8Y-L Micropressure Sensors for Industrial Automation

Annonce de nouveaux produits

Retrouvez-nous sur


Learn more about the E8YL micropressure sensors
Learn more about the E8YL micropressure sensors

January 21, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new E8Y-L micropressure sensors with digital display from Omron Electronics. The E8Y-L devices are compact digital pressure sensors designed to save space and provide clear on-site monitoring for industrial manufacturing equipment and factory automation applications.

The Omron E8Y-L micropressure sensors feature a compact design (31mm × 30mm × 30mm) and an easy-to-read red LED indicator, enabling the monitoring of pressure in various scenarios and different zones. This allows applications such as maintaining regulated pressure in a clean room or automatically regulating ducts or valves. These EN- and UL-approved sensors include analog current output models and pressure port Rc (PT) 1/8 models offering zero-point adjustment, and automatic teaching settings that allow users to set custom pressures at which the sensor turns on or off. Users can set the zero point to any value to simplify tracking pressure changes in semiconductor wafer-processing reactors, monitoring organic gas flow paths during implantation, or in safety systems such as purge gas leakage detection. In addition, users can interact with the device via four simple buttons on the front panel to select the measurement range, displayed channel, operating mode, or set thresholds for the upper and lower limits of measurement pressure, which can simplify the detection of machinery faults, such as clogged exhausts or blocked vents.

The E8Y-L sensors operate from -10°C to 55°C, with no condensation or icing, and can withstand up to 85% relative humidity, making them suitable for use in a wide variety of industrial environments. With a wide supply voltage range of 12V to 24V and a current consumption of up to 50mA or 75mA, the sensors are ready to operate from popular industrial power rails. The E8Y-L sensors were featured in a recent Mouser "New Tech Tuesday" blog.

To learn more about the E8YL micropressure sensors, visit https://www.mouser.com/new/omron-electronics/omron-e8y-l-micropressure-sensors/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

À propos de Omron

2026 - Omron est le premier fournisseur mondial de composants électroniques de pointe. La vaste gamme de produits d'Omron comprend des commutateurs (généraux, à action instantanée, de contrôle, DIP/SIP, miniatures, sous-miniatures et à molette), des relais, connecteurs, optoélectronique et des capteurs qui sont utilisés dans l'électronique grand public, les périphériques informatiques, les produits d'automatisation de bureau et les applications de télécommunications. Omron Industrial Automation fournit au monde entier des composants électroniques et des composants de système de contrôle avancés, notamment des commutateurs, relais, alimentations, capteurs, équipements d'étalonnage et ensembles de câbles. Omron est un leader mondial de la technologie RFID avec sa large gamme de produits et de systèmes fiables, tels que les inlays, les lecteurs/écrivains, les transpondeurs, les outils de développement et les accessoires.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764