Mouser Stocks Broad Lineup of RF, CATV, and Radar Products from Qorvo
June 15, 2021 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, stocks a broad range of Qorvo® products, including RF power amplifiers, filters, and application controllers, suitable for a wide variety of cellular infrastructure, satellite, and cable TV (CATV) applications.
Qorvo product highlights available from Mouser include:
- Qorvo QPA2575 Ka-Band Power Amplifier: This fully integrated and 50-ohm impedance matched SMD amplifier provides a 19 dB small-signal gain to deliver up to 3 watts output power in the range 32 GHz to 38 GHz. The input and output include DC blocking capacitors.
https://www.mouser.com/new/qorvo/qorvo-qpa2575-power-amplifier/ - Qorvo QPA2310 C-Band 50W GaN Power Amplifier: The GaN-based 50 W QPA2310 RF power amplifier is packaged in a QFN format and provides a +23 dB gain with up to 53% power added efficiency. Designed for applications operating in the 5 GHz to 6 GHz C-band spectrum, all input and output matching components are integrated within the device, saving board space and weight.
https://www.mouser.com/new/qorvo/qorvo-qpa2310-cband-50w-gan-amplifier/ - Qorvo QPA2309 C-Band 100W GaN Power Amplifier: Based on Qorvo’s QGaN25HV process, the 100 W QPA2309 operates in the 5 GHz to 6 GHz C band and includes all matching components and delivers up to +22 dB gain with a 52% power added efficiency.
https://www.mouser.com/new/qorvo/qorvo-qpa2309-cband-100w-gan-amplifier/ - Qorvo QPL181x Suite of CATV Amplifiers: The QPL181x series ICs are single-ended, matched, 75-ohm, low-noise, small-signal GaAs RF amplifiers designed specifically in use in cable modems, FTTH infrastructure, DOCSIS 4.0, and set-top box applications operating in the 50 MHz to 1800 MHz frequency range. The small signal gain characteristics across the series is typically 15 dB.
https://www.mouser.com/new/qorvo/qorvo-qpl181x-catv-amplifiers/ - Qorvo QPQ1298 High-Performance BAW Filter: Designed specifically for the 160 MHz bandwidth sub-band 41 uplink and downlink applications, the bulk acoustic wave (BAW) filter features a low insertion loss of 2.5 dB and an attenuation characteristic better than +30 dB and up to +46 dB in the Wi-Fi range.
https://www.mouser.com/new/qorvo/qorvo-qpq1298-baw-filter/
For more information about Qorvo, visit https://www.mouser.com/manufacturer/qorvo/.
Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.
2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.
Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.