Qorvo Wi-Fi 7 Front End Modules, New at Mouser, Deliver Wireless Connectivity for Mobile and Home Network Equipment
April 24, 2025 – Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is now shipping the newest Wi-Fi® 7 front end modules (FEM) from Qorvo, designed for customer premises equipment, smart home devices, portable consumer electronics and wearables.
Wi-Fi 7 is the newest Wi-Fi standard, also known as IEEE 802.11be Extremely High Throughput (EHT). Wi-Fi 7 works across three separate bands (2.4 GHz, 5 GHz, and 6 GHz) to fully utilize spectrum resources. Wi-Fi 7 offers faster data speeds, lower latencies, and increased network capacity thanks to new capabilities designed to provide exceptional performance and support large numbers of users and devices in bandwidth-intensive environments.
The Qorvo QM45655, available from Mouser, integrates a multi-transmit-state 5 GHz to 7 GHz frequency power amplifier. The QM42655 integrates a multi-transmit-state 2.4 GHz Wi-Fi power amplifier that is also used for high-performance Bluetooth (HP BT). These devices are optimized for a broad 3 V to 5 V operating range, making them ideal for mobile applications such as smartphones and tablets and wearables such as VR/AR goggles.
The QPF4509 and QPF4609 are Wi-Fi 7 front end modules well suited for wireless access points, wireless routers, set-top boxes and customer premise equipment. The QPF4509 offers a 5.17 GHz to 5.895 GHz frequency range, while the 4609 provides a 5.925 GHz to 7.125 GHz range. These devices include integrated power amplifiers, low noise amplifiers and switches optimized for operation at 5V. This design conserves power consumption while maintaining the highest linear output power and leading-edge throughput.
Qorvo's QM45655EVB01, QM42655EVB, QPF4509EVB, and QPF4609EVB evaluation boards, also available to order from Mouser, provide a demonstration and development platform for these Wi-Fi 7 modules. Each board features a pre-mounted target device, along with the required support circuitry. These evaluation boards provide an example application circuit, allowing rapid prototyping when incorporated into existing designs.
To learn more about the QM45655 and QM42655 mobile Wi-Fi FEMs, visit https://www.mouser.com/new/qorvo/qorvo-qm45655-fem and https://www.mouser.com/new/qorvo/qorvo-qm42655-fem/.
To learn more about the QPF4509 and QPF4609 network equipment FEMs, visit https://www.mouser.com/new/qorvo/qorvo-qpf4509-modules/ and https://www.mouser.com/new/qorvo/qorvo-qpf4609-modules/.
To learn more about Qorvo Wi-Fi 7 modules available from Mouser, visit https://www.mouser.com/new/qorvo/qorvo-wi-fi-7-modules/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.
2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.
Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.