Mouser Electronics Signs Distribution Agreement with Industrial Control Specialist Weintek

Pour publication immédiate

Retrouvez-nous sur


Learn more about Weintek
Learn more about Weintek

November 10, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, announces a global distribution agreement with Weintek, a leading global supplier of industrial automation control devices. Through the agreement, Mouser now offers the Weintek product line of human-machine interface (HMI), IIoT, and I/O solutions.

The Weintek cMT-X series LCD touch panels, now available from Mouser, are designed to provide a full-featured human-machine interface. Ideal for industrial automation, machine control, and self-service kiosks, these touch panels help businesses accelerate smart manufacturing and streamline data-driven management. The cMT-X series is available in standard and advanced versions to address different requirements. These HMI devices feature quad-core CPUs, a wide 178° viewing angle, up to 4GB flash, up to 1GB RAM, and built-in connectivity with over 400 communication drivers.

The M02 Wi-Fi® module, also available from Mouser, is designed to work with the cMT2108X2 and cMT3102X touch panels, adding wireless connectivity in hard-to-wire environments. The M02 module features a compact design, adding little protrusion when installed on the HMI, avoiding space issues in control cabinet installations. The module includes an external magnet-mounted antenna for ease of use and optimal signal.

The cMT-SVR faceless HMIs are designed to enable users complete control using an app from a phone, tablet, or PC over a Wi-Fi or LAN connection. Powered by license-free development software, EasyBuilder Pro, and with support for over 400 industrial protocols, the Faceless HMI is designed for simplicity and flexibility. The faceless HMIs come with a built-in power isolator and feature one USB host port and a Gigabit Ethernet port.

Weintek's iR series I/O modules are a remote I/O modular system designed for flexible and scalable industrial automation. Compact and DIN rail-mountable, the iR modules integrate easily with HMIs and controllers. The iR I/O modules support a wide range of communication protocols, including EtherNet/IP, Modbus TCP, EtherCAT, and CANopen. These modules come in digital I/O, analog I/O, and temperature variants.

To learn more about Weintek, visit https://www.mouser.com/manufacturer/weintek/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

À propos de Weintek

2026 - Weintek specializes in HMIs, IIoT solutions, and I/O. These products undergo meticulous design and testing to meet and exceed UL and CE compliance standards. With ISO9000 certification, this company manufactures products using advanced equipment, professional techniques, and standardized processes, ensuring both reliability and optimal product efficiency.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764