Infineon's BGT60ATR24C XENSIV 60GHz Radar MMIC, Now Available at Mouser, Detects In-Vehicle Occupancy

Annonce de nouveaux produits

Retrouvez-nous sur


November 28, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the BGT60ATR24C XENSIV™ 60GHz radar monolithic microwave integrated circuit (MMIC) from Infineon Technologies. Using ultra-wide bandwidth Frequency-Modulated Continuous-Wave (FMCW) operation, the BGT60ATR24C can address numerous passive safety applications like child detection, driver monitoring, and occupancy sensing due to its ability to sense micro motions aesthetically. The BGT60ATR24C has been designed for ultra-short-range applications with best-in-class jitter performance, ultra-low power consumption, wideband operation and robustness, and is ideal for in-cabin automotive monitoring systems.

The Infineon Technologies BGT60ATR24C, now available at Mouser, is a fully integrated radar transceiver operating in the frequency band from 58 GHz to 62 GHz. It is a state-of-the-art radar chip featuring two transmit channels, four receive channels, a low noise Phase Locked Loop (PLL), an integrated anti-aliasing Loop Filter (LF), a sequencer and finite state machine for ramp generation, an integrated RX baseband including analog to digital conversion (ADC), sensor ADCs for temperature and power monitoring, all within a single chip. The digitized time signals are forwarded via the SPI interface to the application controller, where they can be processed further. The BGT60ATR24C features a digital interface for sensor configuration and data acquisition, as well as an integrated state machine for independent data acquisition. The radar MMIC includes optimized power modes for low power consumption.

The BGT60ATR24C XENSIV 60GHz Radar MMIC is supported by the SHIELD_60ATR24ES_01 demo board. The SHIELD_60ATR24ES_01 features a pre-mounted BGT60ATR24C in a 6 mm x 6 mm package, along with support circuitry and an onboard L-shaped antenna. This demo board enables prototyping for various use cases, including presence detection, proximity sensing, people counting and tracking, gesture recognition, monitoring vital signs and more.

To learn more about the Infineon Technologies BGT60ATR24C XENSIV 60GHz radar MMIC, visit https://www.mouser.com/new/infineon/infineon-bgt60atr24c/.

To learn more about the SHIELD_60ATR24ES_01 demo board, visit https://www.mouser.com/new/infineon/infineon-shield-60atr24es-01-board/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

À propos de Infineon Technologies

2026 - Infineon Technologies est un concepteur, fabricant et fournisseur mondial de premier plan d’une large gamme de semiconducteurs utilisés dans diverses applications microélectroniques. Le portefeuille de produits Infineon se compose de produits logiques, notamment de circuits intégrés numériques, à signaux mixtes et analogiques, ainsi que de produits semi-conducteurs discrets.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764