STMicroelectronics' STUSB4531 Standalone USB PD Controller, Now at Mouser, Simplifies the Development of USB Type-C Sink Devices

Annonce de nouveaux produits

Retrouvez-nous sur


Learn more about the STUSB4531 USB PD controller
Learn more about the STUSB4531 USB PD controller

April 23, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the STUSB4531 standalone SINK USB PD controller from STMicroelectronics. The STUSB4531 is the industry's first USB PD 3.2 sink controller to offer a hybrid mode. The STUSB4531 PD controller simplifies the development of battery-charging and VBUS-powered electronics in set-top boxes, cameras, healthcare and handheld devices, LED lighting, and any other type-C/PD sink device. The STUSB4531 is also ideal for USB micro-B and DC barrel replacement.

The STMicroelectronics STUSB4531 USB PD controller, now at Mouser, includes a hardwired USB PD stack that implements proprietary algorithms to enable software-free negotiation. This feature makes the STUSB4531 suitable for automatic high-power profile charging, especially from a dead battery power state. The STUSB4531 also offers a hybrid mode that supports full-feature applications with a minimal external software layer, simplifying the implementation of optional USB PD features. In hybrid mode, an external application processor can interact with the stack and leverage the USB PD communication protocol layers, enabling engineers to implement alternate modes, battery messaging, data role swapping, and vendor-defined messages (VDM).

The STUSB4531 controller enables the adoption of USB-C for charging and powering devices, in line with international mandates to reduce electronic waste. The STUSB4531 USB PD controller is certified to the latest USB Type-C® 2.4 and USB PD 3.2 standards, as well as to IEC 62680 for EU conformity. Developers using the STUSB4531 controller can leverage the STMicroelectronics EVAL-SCS007V1 evaluation board and the EVAL-SCS006V1 reference design.

To learn more, visit https://www.mouser.com/new/stmicroelectronics/st-stusb4531-sink-usb-pd-controller/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764