Mouser Electronics Now Stocking Maxim MAX17250 DC-DC Boost Converter with 0.1 μA True Shutdown Mode
November 19, 2018 - Mouser Electronics, Inc. the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the MAX17250 DC-DC synchronous boost converter from Maxim Integrated. The MAX17250 offers up to 93 percent efficiency to minimize heat dissipation, with an ultra-low quiescent current that helps extend battery life in digital cameras, battery-powered Internet of Things (IoT) devices, and other connected designs.
The Maxim MAX17250 DC-DC boost converter, available from Mouser Electronics, includes a selectable input peak current limit of 3.5 A, 2.7 A, or 1.85 A and operates over an input voltage range of 2.7 V to 18 V with an output voltage range of 3 V to 18 V. The device supports switching frequencies up to 1 MHz and offers short-circuit protection and a maximum on-time of 800 ns in a space-saving 12-bump, 1.72 mm × 1.49 mm package.
The MAX17250 converter implements three modes of operation: The first mode of operation is a soft-start mode at power-up. The second mode of operation is normal operation, which uses a fixed on-time/minimum off-time pulse frequency modulation (PFM) architecture that uses only 60 μA (typical) quiescent current due to the converter switching only when needed. The MAX17250 converter's True Shutdown™ mode completely disconnects the output from the input, resulting in a current draw of just 0.1 μA, virtually stopping battery drain, providing long battery life, and eliminating the need for external disconnect switches.
Mouser is also stocking the Maxim MAX17250EVKIT#WLP evaluation kit, a fully assembled and tested kit that incorporates the MAX17250 converter and provides resistor-configurable output voltages from 3 V to 18 V.
To learn more, visit www.mouser.com/maxim-max17250-converter.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 750 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Maxim Integrated
Maxim is the leader in analog integration. From mobile to industrial solutions, Maxim is making analog smaller, smarter and more energy efficient.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com