Now at Mouser: Texas Instruments' ADS7057 SAR ADC Offers High-Speed Data Acquisition at Low Power
April 10, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the ADS7057 successive-approximation register (SAR) type analog-to-digital converter (ADC) from Texas Instruments (TI). The ADS7057 ADC dissipates only 3.6 mW at a maximum sampling rate of 2.5 megasamples per second (MSPS) and only 0.02 µW when static.
The TI ADS7057, available from Mouser Electronics, is a 14-bit, single-ended input, SAR ADC with a range of 0V to AVDD, and AVDD in the range of 2.35 V to 3.6 V. Ideal offset specifications over the entire AVDD and temperature operating range is maintained through the internal offset calibration. The ADS7057 supports an SPI-compatible serial interface controlled by the CS and SCLK signals. The device uses an input signal that is sampled with the CS falling edge, and SCLK is used for both conversion and serial data output. A wide digital supply range of 2.35 V to 3.6 V is enabled on the ADS7057, directly interfacing to a variety of host controllers. A normal DVDD range of 1.65 V to 1.95 V allows the ADS7057 to comply with the JESD8-7A standard. The 8-pin, 1.5 mm × 1.5 mm device features an extended industrial temperature range of minus 40 to 125 degrees Celsius and is ideal for space-constrained and battery-powered applications that require high-speed, high-resolution data acquisition, such as optical encoders, sonar receivers, ultrasonic flow meters, and handheld cameras.
The ADS7507 ADC is supported by the ADS7057EVM-PDK Performance Demonstration Kit, which provides the hardware and software required for diagnostic testing of the ADC. The kit includes the ADS7057 EVM board and the precision host interface (PHI) controller board, which enables the accompanying computer software to communicate with the ADC over USB for data capture and analysis.
To learn more, visit www.mouser.com/ti-ads7057-adcs.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 22 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com