Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

TI's LDC1101 1.8V Inductance-to-Digital Converter, Now at Mouser, Targets High-Speed Measurement Systems

August 31, 2015 - Mouser Electronics, Inc. is now stocking the LDC1101 inductance-to-digital converter (LDC) from Texas Instruments (TI). The LDC1101 is a 1.8V to 3.3V, high-resolution data converter designed for short-range, high-speed, contactless sensing of position, rotation, or motion. The LDC1101 provides accurate measurements in both controlled and harsh environments, making it ideal for automotive, consumer, industrial, computer, and communications applications.

The TI LDC1101 inductance-to-digital converter, now available from Mouser Electronics, features dual inductive measurement cores, allowing for 16-bit resonator resistance (RP) and inductance (L) measurements at more than 150 Ksps. Simultaneously, the converter can perform 24-bit-resolution inductance measurements at more than 180ksps. The LDC1101 includes a threshold-compare function which can be dynamically updated while the device is running, greatly simplifying designs such as high-speed gear counting.

The LDC1101 supports a wide range of inductor/capacitor (LC) combinations with oscillation frequencies ranging from 500kHz to 10MHz and RP ranging from 1.25 kΩ to 90 kΩ. The device is configured and conversion results retrieved through a simple 4-wire SPI. The only external components necessary for operation are a 15nF capacitor for internal LDO bypassing and supply bypassing for VDD.

TI's LDC1101EVM evaluation module, also available from Mouser Electronics, allows designers to test and demonstrate inductive sensing technology using the LDC1101 device. The evaluation board includes an example PCB sensor coil that connects to the LDC1101. Designers can use the onboard TI MSP430 microcontroller to interface the LDC to a host computer. This module is designed to provide the user with maximum flexibility for system prototyping.

To learn more, visit http://www.mouser.com/new/Texas-Instruments/ti-ldc1101-converter/.


With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

About Texas Instruments
Texas Instruments Incorporated designs and manufactures analog technologies, digital signal processing (DSP) and microcontroller (MCU) semiconductors. TI is a leader in semiconductor solutions for analog and digital embedded and applications processing. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, visit http://www.ti.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room